If the pk-pk ripple current is set to 10% at the max output current level, then at 50% analog dimming is it 10% or 20%?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If the pk-pk ripple current is set to 10% at the max output current level, then at 50% analog dimming is it 10% or 20%?
Hello Sam,
The current ripple is a function of the LED stack voltage not the output current. If the peak to peak current ripple is 10% at 100% analog dimming then it will be close to 20% peak to peak at 50%. The average output current will not be half of 100% because the TPS92518 regulates peak current. This means when analog dimming is set to 50% the average output current will be less than 50%.
Regards,
Thanks Irwin,
So, how would we set up this part if the driver requirement is such that it can be programmed from 100mA to 1A, 2V to 55V Led forward voltage and less than 30% pk-pk ripple, assuming TPS92518HV and 60Vdc input?
One way is to set the pk--pk ripple at 3% at 1A. Is this the only way?
Regards