Hi dear supporting team,
my customer use SN47LVC1G3157 for the GSCLK switching for TLC5943, the sch is as attached below: sn47lvc1G3157 ON-State Resistance:6ohm(TYP)Switch Capacitance:17.4pF (TYP),could you help confirm from osc output which marked as 1 in the sch, to 2, will there be any impedance match issue which will affect TLC5943 GSCLK? because there is few description on GSCLK requirement in TLC5943 sch, but GSCLK as PWM control , the actual loading is not very sensitive to PWM frequency jittering. tks a lot!