HELLO TEAM ,
Greetings!!!
We are looking for constant current led driver which must have following specification:
Input voltage range : 22 to 25 volt dc
Output voltage : 5W to 15W with constant current 350mA ( buck as well as boost
Efficiency : 85% to 90%
Dimmable with Microprocessor Please suggest me corresponding IC and design resource available.
Regards Rahul
Have you reveiwed the available reference designs in the PowerLab reference design datasbase? You can find it a www.ti.com and then click on "power management"