• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Power Management » LED Drivers/LCD Bias » LED Drivers/LCD Bias Forum » TLC5947 24-bit LED driver question about setting current
Share
LED Drivers/LCD Bias
  • Forum
  • Announcements
  • E2E Wiki
Options
  • Subscribe via RSS

Forums

TLC5947 24-bit LED driver question about setting current

This question is answered
Jonathan Slaughter
Posted by Jonathan Slaughter
on Jul 09 2009 00:05 AM
Prodigy70 points

(Not sure if this is the appropriate forum but I couldn't find any other place to post this)

The TLC5947 uses a pin to set the current which determines the global led intensity.  I am cascading several of these devices and would like to use one common iref to reduce the resistors needed and have an easy way to set the led intensity across all the ic's(using one pot instead of many). Is it safe to do this? Of course I would have to increase the resistance by a factor of the number of IC's used.  I could add a small resistance to each iref to help with current sharing if necessary. This might be ideal as I would like to limit current as well but I would also like to minimize components as board space is a bit tight.

Report Abuse
  • Reply
You have posted to a forum that requires a moderator to approve posts before they are publicly available.
All Replies
  • Michael Day
    Posted by Michael Day
    on Jul 20 2009 09:37 AM
    Suggested Answer
    Mastermind36070 points

    No this is not possible. Pin R-EXT is basically the output of a voltage reference. Refernce voltages can not be paralleled. There is a resistor from R-EXT to GND needed for each LED driver.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Jonathan Slaughter
    Posted by Jonathan Slaughter
    on Jul 20 2009 10:09 AM
    Suggested Answer
    Prodigy70 points

    Are you 100% sure that they cannot be paralleled? I understand that if it is a voltage reference that they cannot but are you sure that the IC uses some type of voltage reference design? What if I were to put some small resistors in series with each device then all to a larger resistor? The small resistors act as current limiting but also allow for the differences in voltage drops to occur between devices.

     

    TLC1->IREF1->R1->R->Gnd

    ...

    TLCn->IREFn->Rn->R->Gnd

     

    (R1 through Rn will have the same magnitude but are physically different while R is the same resistor)

     

    This is actually how I have designed the circuit. R1 through Rn will have the value that gives the maximum current I want and increasing R will allow me to reduce the current for global intensity. I believe this should work as I'm simply lifting the ground w.r.t. to iref. But each iref has it's own resistor also.

     

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Michael Day
    Posted by Michael Day
    on Jul 20 2009 11:46 AM
    Verified Answer
    Verified by Jonathan Slaughter
    Mastermind36070 points

    My mistake.  If you use a separate resistor for each TLC5947 and then connect all these resistors together to a common variable resistor, you can configure your system so that changing the common resistor changes the global constant current value.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Jonathan Slaughter
    Posted by Jonathan Slaughter
    on Jul 20 2009 16:17 PM
    Prodigy70 points

    Thanks. I was not clear but I think I've got the information I needed now.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Jonathan Slaughter
    Posted by Jonathan Slaughter
    on Jul 23 2009 18:14 PM
    Prodigy70 points

    One more quick question(which might be somewhat dumb but I just want to be absolutely sure before I send off these boards).

     

    The TLC5947 will work just fine if only some of the outputs are used and the others are not connected at all?  Do I have to set the greyscale code for those to 0 or will everything be fine in any condition?

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Michael Day
    Posted by Michael Day
    on Jul 24 2009 10:27 AM
    Verified Answer
    Verified by Jonathan Slaughter
    Mastermind36070 points

    You can operate the IC with unused outputs left open.  However, if the unused outputs are programmed to sink current but are opened, the IC will draw additional input current as it tries to provide a higher drive current to the unused outputs.  This will not damage the IC, but results in higher power dissipation.  You can eliminate this additional current by programming all unused outputs to sink 0mA of current.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
  • Jonathan Slaughter
    Posted by Jonathan Slaughter
    on Jul 24 2009 15:50 PM
    Prodigy70 points

    Thank you.

    Report Abuse
    • Reply
    You have posted to a forum that requires a moderator to approve posts before they are publicly available.
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use