Hello,
we want to use the LP8501 or the LP55231 to drive some white µLEDs. The LEDs should be switched On/Off with a frequency around 2kHz. If I understand the datasheet correctly the PWM frequency is 312Hz. Is there a way to change that value manually? If not is the driver still capable to drive the LED, disregard the PWM function, with the desired settings?
Regards,
Florian E.