I need to deisgn a LED Drive circuit (SMPS) which can drive two different LED luminaires which may be connected to it:-
One luminaire is 6 LEDs in series with 330mA current.
The other luminaire is one LED with 650mA current.
The above 330mA must be dimmable down to 22mA (+/- 20%)
The above 650mA LED must be dimmable down to 65mA (+/- 5%)
My supply rail voltage is 14V (+/- 20%).
(it pulsates at 100Hz due to baing secondary of mains power supply)
The LED luminaires will be attached to the LED driver by three metres of cable, so we must put considerable capacitance across the connection to the cable in the LED Driver…
…….we are also worried about EMI from this cable –specially wondering about how PWM type dimming would affect EMI from this cable.
Initial investigations with buckboosts, show that the LED current tends to oscillation if not addressed, and also that supply ripple rejection requires much work with the control loop.
Do you have LED Driver IC’s for this ?