• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Power Management » LED Drivers/LCD Bias » LED Drivers/LCD Bias Forum » All Tags » TLC59xx
Share
LED Drivers/LCD Bias
  • Forum
  • Announcements
  • E2E Wiki

Browse by Tags

LED Drivers/LCD Bias

Welcome to the LED Drivers/LCD Bias Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Sign In to Post
Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
TLC59xx
  • buffer
  • cascade
  • dissipation
  • impedance load
  • interface
  • Lighting
  • MSP430
  • power
  • power dissipation
  • SDA
  • Signage products
  • system efficiency
  • temperature protection
  • TLC59025
  • TLC59108
  • TLC59116
  • TLC5916
  • TLC5920
  • TLC5926
  • TLC5927
  • TLC5947
  • TLC5951
  • TLC5952
Related Posts
  • Forum Post: Re: TLC5927 / power dissipation

    Brigitte Brigitte
    Hello Carl, The biggest portion will be the power dissipation caused by the LED currents. The TLC5927 has to dissipate the power coming from the LED power supply through the diodes to GND which is not taken from the LEDs, therefore for all 16 outputs the maximum power dissipated per output will be...
    on Jul 26, 2010
  • Forum Post: Re: TLC5925 / 59025

    Brigitte Brigitte
    Hello Jan, 1. TLC59025 also uses the industry standard for Iout to external resistor ratio. 2. We never tested the parts with other loads than LEDs. In general I would say that the impedance limits the current, even if the IC wants to draw more current. I do not expect the drivers to oscillate...
    on Aug 12, 2010
  • Forum Post: Re: LED signage

    Brigitte Brigitte
    Hello Abhishek, A good place to start your search is this web page: http://www.ti.com/led . One of the TLC59xx parts will most probable be the right part for you application. Best regards, Brigitte
    on Nov 9, 2010
  • Forum Post: MSP430G2231 Interfacing with TLC 5940 for 7 x 5 LED Matrix

    Sascha Walther Sascha Walther
    Hello, I'm quite new to microcontrollers and have started working with the Launchpad and am therefore restricted to the Value Line of the MSP430 MCU's. I want to connect 2 LED Panels with 7 x 5 Leds each which are internally connected through a matrix. My question is if there is existing...
    on Jan 23, 2011
  • Forum Post: Re: Looking for some advice for 8x8 RGB Led matrix driver

    Brigitte Brigitte
    Hello Amid, The only possibilities I know of to avoid timing is a good layout and adding a buffer every few parts in all lines which are not buffered in the TLC59xx. It is for sure the case that you will see after some ICs a time and slope difference between the signals that are buffered in the ICs...
    on Jun 3, 2011
  • Forum Post: Re: TLC + MSP430

    Brigitte Brigitte
    Hello Raul, Do you mean generating the driver software for one of the TLC59xx parts? I am not a programming expert, but I am told that the interfaces of all parts are simple and you just have to make sure that the timings are correct. Normally GPIOs or even existing interfaces can be used (dependent...
    on Aug 4, 2011
  • Forum Post: TLC5920 possible timing or current leakage problem

    Josh Triska Josh Triska
    Hello, I have a design for a client which uses four cascaded TLC5920 chips driving one 16x8 LED matrix each. My issue is that on rows which have, say, one LED lit, the other LEDs in the same row (on the same COM pin) glow faintly. Order of operations to write to the four chips: Pull blank high...
    on Apr 14, 2011
  • Forum Post: Re: MBI5028 analog

    Oleksiy Pazyuk Oleksiy Pazyuk
    Hello . Do you know if TLC59281 TLC59282 have temperature shutdown. I was not able to find this information in the datasheet? For TLC59025/TLC5926 / TLC5927 there is overtemperature shutdown at 175C Does it mean that for TLC59281/ TLC59282 there is no any temperature protection? best regards...
    on Oct 27, 2011
  • Forum Post: TLC59116 / TLC59108 SDA held low issue

    Bernard McDavitt Bernard McDavitt
    Hi, I am currently work on a project to control multiple TLC59116 / TLC59108 an have come across a problem where noise induced on the lines is occasionally causing one or possibly more of the devices to hold the SDA line low indefinitely. The devices are connected in a 'star' configuration...
    on Nov 24, 2011
  • Forum Post: Re: TLC5952/51/47 Power Efficiency

    Brigitte Brigitte
    Hello Himansu, These parts are not power converters. The input power has to come from another power IC. The TLC5951, TLC5952 or TLC5947 just connect external LEDs to GND and regulate the current through the LEDs. The OUTx pins are current sinks that regulate the current. In the datasheets you can...
    on Dec 19, 2011
  • Forum Post: TLC5916 output state retention issue.

    Olivier Nsabimana Olivier Nsabimana
    Hi, I am using two cascaded TLC5916 chips to drive 12 LEDs, mixed green and red. this is a very straight forward task, which doesn't require brightness control or anything like, just turning on LEDs and OFF as required. My implementation is as follow. I use a 16 bit field variable ( uint16_t...
    on Feb 12, 2013
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use