• Join
  • Sign In with my.TI Login
Texas Instruments
  • Products
  • Applications
  • Tools & Software
  • Support & Community
  • Sample & Buy
  • About TI
Sample & Purchase Cart Sample & Purchase Cart
  • Search
  • Advanced
TI E2E™ Community
  • Support Forums
  • Blogs
  • Groups
  • Videos
  • 简体中文
  • More ...
TI Home » TI E2E Community » Support Forums » Power Management » LED Drivers/LCD Bias » All Tags » led driver
Share
LED Drivers/LCD Bias
  • Forum
  • Announcements
  • E2E Wiki

Browse by Tags

LED Drivers/LCD Bias

Welcome to the LED Drivers/LCD Bias Section of the TI E2E Support Community. Ask questions, share knowledge, explore ideas, and help solve problems with fellow engineers. To post a question, click on the forum tab then "New Post".

Tags
You have subscribed to this tag. To view or manage your tag subscriptions, click here.   Close
You have unsubscribed from this tag. To view or manage your tag subscriptions, click here.   Close
You are currently viewing:
led driver
  • constant current
  • current
  • current limit
  • dimming
  • Dot Correction
  • GSCLK
  • LED
  • LED Array
  • lighting
  • Output current
  • power dissipation
  • PWM dimming
  • TL4242
  • TLC59108
  • TLC59116
  • TLC5926
  • TLC5940
  • TLC59401
  • TLC5941
  • tlc5943
  • TLC5947
  • TLC5951
  • tlc5960
  • TLC5971
  • tps61500
Related Posts
  • Forum Post: Re: LED Driver IC needed for demanding application

    Michael Day Michael Day
    I suggest the TPS54160 EVM as a good starting point. http://focus.ti.com/docs/toolsw/folders/print/tps54160evm-535.html
    on Feb 4, 2010
  • Forum Post: TLC59108 - Output Voltage ? Leakage Current ?

    Hiroshi Hashimoto41395 Hiroshi Hashimoto41395
    Does the output of this device allow the applied voltage up to 17V or 20V at VCC=0V? And, what is value of the output leak current at that time?
    on Feb 10, 2010
  • Forum Post: Re: TLC59108

    Hiroshi Hashimoto41395 Hiroshi Hashimoto41395
    Thank you very much. I learnt now that the VO(MAX) SPEC of TLC59108 was meaning different from VO(MAX) SPEC of the data sheet of a standard logic product. And, I learnt that the TLC59108 is not able to using for partial power-down application. Thanks again.
    on Feb 12, 2010
  • Forum Post: Re: TLC59108 SAMPLE PROGRAM

    Hiroshi Hashimoto41395 Hiroshi Hashimoto41395
    I understood. In other LED drivers in the past. I saw the case of not able to operation correctly with order of register setting flow. The order had not been described to the data sheet. Therefore, I wanted a standard flow of the register setting that became the most basic, the illumination pattern...
    on Feb 12, 2010
  • Forum Post: Re: TLC59108 SAMPLE PROGRAM

    Subodh Nijsure Subodh Nijsure
    I second the request it would be nice if there was a sample or even a script that showed how to setup things, reset using standard i2c-tools (i2cset). There must be someone in TI that has already done this to test the device, no?
    on Mar 18, 2010
  • Forum Post: TPS61165 PWM control

    Shannon Shannon
    Hi, I'm using a TPS61165 to drive high brightness LEDs, and I'm not sure from the datasheet how the PWM control works. I'm hoping to flash the LEDs at a low frequency (visible to the human eye, so less than 60 Hz), and vary the dimming at the same time to create an interesting display for...
    on Mar 23, 2010
  • Forum Post: Output Current TLC59116

    Alexandre Marcotte Alexandre Marcotte
    I want to know if the tlc59116 have a maximum of 100 mA for each OUTPUT of 100 mA for all OUTPUT. I use 14 output lines with 20 mA leds How I can calculate the disipate power in the Rext Thank you! Sorry for my english Alexandre Marcotte Student at the University Of Sherbrooke
    on Jun 1, 2010
  • Forum Post: LED driver to illuminate for video camera

    Elliott Johnson Elliott Johnson
    I need a LED driver that can power a sting of LEDs which will illuminate an area that can range from pitch black to well lit (LEDs off). The device will be battery powered, but due to the limitations of the camera module the control unit and camera module will have to use the same power source, that...
    on Jul 23, 2010
  • Forum Post: LED lighting for commercial appliactions

    RUJAL ANGADIA54345 RUJAL ANGADIA54345
    Can anyone provide complete board details of PMP4501 ref design including transformer construction, gerber layout, BOM & schematic ? The overview can be found on page no 18 of Reference Design Cookbook labeled as slyt394a.. Thanks in advance
    on Jul 31, 2010
  • Forum Post: Re: LED lighting for commercial appliactions

    RUJAL ANGADIA54345 RUJAL ANGADIA54345
    Here also does not contains no of turns in any of windings without which Xmer cannot be manufactured & the gerber file is not extractable.
    on Aug 2, 2010
  • Forum Post: Re: Configuring TLC59401 using FPGA

    Brigitte Brigitte
    Hello Praveen, What do you mean with architecture? For a lot more technical information then in the TLC59401 product folder, please review the EVM document and the application notes you can find in the TLC5940 product folder. Maybe this helps to solve your issues. TLC5940 and TLC59401 are almost identical...
    on Aug 18, 2010
  • Forum Post: Re: searching for LED driver

    Michael Day Michael Day
    The TPS61086 datasheet has good information that will help you understand the available output current at different input voltages and currents. Please refer to figure 8 and go through the datasheet design procedure. Output current is much less than the peak switch current. You need to define the input...
    on Sep 2, 2010
  • Forum Post: TLC5941 to MPU timing madness

    Chuck Begian Chuck Begian
    Perhaps software engineers should not be put on hardware design projects. I am at my wits' end with this thing. Here is what I am trying to do... I have 4 TLC5941s cascaded to drive a dot-matrix LED display. The data for each row of the display is shifted into the TLC5941s, latched, and then...
    on Oct 15, 2010
  • Forum Post: TPS61161 blows on LED disconnect

    G��nter Thelen-Piazzolla G��nter Thelen-Piazzolla
    Dear sirs, I have successfully implemented the TPS61161 to drive a string of 9 backlight-LEDs, using the configuration from the datasheet. But after having built 100 units, I have 5 ones on which the TPS61161 had to be replaced (and no component else ). On two occasions the LED string FPC had been...
    on Oct 28, 2010
  • Forum Post: TLC59116 Output current not matched (output wide open)

    joep niermeijer joep niermeijer
    I'm using a TLC59116 in my design, but I'm running into problems. While I thought I'd had everyting correctly designed and initiated, the TLC gave me about 50 mA output instead of the 19~20 I designed for. My setup: -TLC running at 5V -Rext of 1k connected to gnd -initiated TLCs adresses...
    on Nov 16, 2010
  • Forum Post: High Brightness LED IC

    Eric DeYoung Eric DeYoung
    I'm looking to find a (switchmode) constant current source for a LED driver that will be powered off from 2 series Lithium Ion batteries. Normal input voltages will range from 7V-8.4V and the output needs to be able to source up to (and preferably slightly greater than) 1.2A with a LED voltage between...
    on Jan 7, 2011
  • Forum Post: Led drivers for an art project: tps61500 and tps40211

    Alexander Jenal Alexander Jenal
    Hello, I have a question concerning a led driver design for an art project. I need to drive several (76) led stripes. It is planned to switch the stripes one after another in about 20 sec. The stripes are ready-made bought from a supplier. Each stripe has an individual length and consists of several...
    on Jan 14, 2011
  • Forum Post: Re: Led drivers for an art project: tps61500 and tps40211

    Alexander Jenal Alexander Jenal
    Thank you for your reply! In order to avoid problems, I decided to use only the TPS40211. Is there a way to use the Enable and the dimming pin together with a pwm signal, so that there only three input pins per driver (vin, gnd, pwm)? I want to use five tlc59116 or similar to switch and (if needed...
    on Jan 17, 2011
  • Forum Post: TPS92210EVM-613 DIMMING-Conducted EMI

    lubo karamfilov lubo karamfilov
    Hi TI, would you pass the graphics(tables,etc.) of conductet EMI? can you show me any documents,if you had? best regards
    on Feb 8, 2011
  • Forum Post: Re: Help choosing multiplexer for 10-segment LED

    Brigitte Brigitte
    Hello Victor, As far as I understand, you have a serial output that gives 0101 if you want to have 5 LEDs lite, right? If you have a look on TLC5925, you can see that this part has a serial interface, therefore you would not need a serial to parallel translation, you need just something that translates...
    on Feb 21, 2011
  • Forum Post: Connected 16units of TPS61195 via SMBUS

    eli eli
    Looking for application/recomendation how to connect 16pcs of TPS61195 (led Driver),via SMBus.
    on Feb 22, 2011
  • Forum Post: TPS61500 problems

    Andreas Pabst Andreas Pabst
    Dear support team / Dear Community, We have a problem concering the TPS61500. Below you will find a description of our project and our problem. We are working in a project for a diploma thesis. The goal of this project is to build a lamp which is able to emit light in most colors of the...
    on Feb 28, 2011
  • Forum Post: Re: Led driver suitable for breadboard or similar size pcb.

    Michael Day Michael Day
    Texas Instruments make several LED drivers. You can review them by going to www.ti.com and clicking on "Lighting Solutions" http://focus.ti.com/general/docs/gencontent.tsp?contentId=28887 You can purchase an EVM that conains the LED driver IC and all necessary supporting circuitry.
    on Mar 25, 2011
  • Forum Post: LED driver Opportuninty

    Calum Mackinnon Calum Mackinnon
    I have a customer who has the following LED driver specs VIn = 41V-45V Vout = 38V Iout = 350mA to 1.3A He wants PWM dimming and needs high side current sense. Ideally it would be a sub $1 part Do you have any suggestions? Cheers Calum
    on Mar 28, 2011
  • Forum Post: TPS61199 datasheet refers to app note SLVA452 which is not online

    Bryan Busacco Bryan Busacco
    The TPS61199 datasheet refers to app note SLVA452 which is not online. For Loop Compensation, the datasheet refers to SLVA452 " Compensating the Current Mode Boost Converter." This document can not be found on TI's website. I did find an alternate document: "Compensating and...
    on Apr 4, 2011
1234
TI E2E™ Community
  • Support Forums
  • Blogs
  • Videos
  • Groups
  • Site Support & Feedback
  • Settings
TI E2E™ Community Groups
  • TI University Program
  • Make the Switch
  • Microcontroller Projects
  • Motor Drive & Control
Other Communities
  • Deyisupport
  • Designsomething.org
  • beagleboard.org
  • TI on Element 14
  • TI on TechXchangeSM
Other Technical & Support Resources
  • WEBENCH® Design Center
  • Product Information Centers
  • Technical Documents
  • TI Design Network
  • TI Technical Articles
  • TI Training

All content and materials on this site are provided "as is". TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with regard to these materials, including but not limited to all implied warranties and conditions of merchantability, fitness for a particular purpose, title and non-infringement of any third party intellectual property right. TI and its respective suppliers and providers of content make no representations about the suitability of these materials for any purpose and disclaim all warranties and conditions with respect to these materials. No license, either express or implied, by estoppel or otherwise, is granted by TI. Use of the information on this site may require a license from a third party, or a license from TI.

Content on this site may contain or be subject to specific guidelines or limitations on use. All postings and use of the content on this site are subject to the Terms of Use of the site; third parties using this content agree to abide by any limitations or guidelines and to comply with the Terms of Use of this site. TI, its suppliers and providers of content reserve the right to make corrections, deletions, modifications, enhancements, improvements and other changes to the content and materials, its products, programs and services at any time or to move or discontinue any content, products, programs, or services without notice.

Follow Us Texas Instruments on Facebook Texas Instruments on Twitter Texas Instruments on LinkedIn Texas Instruments on Google+
TI Worldwide | Contact Us | my.TI Login | Site Map | Corporate Citizenship | mobile m.ti.com (Mobile Version)

TI is a global semiconductor design and manufacturing company. Innovate with 100,000+ analog ICs and
embedded processors, along with software, tools and the industry’s largest sales/support staff.

© Copyright 1995-2013 Texas Instruments Incorporated. All rights reserved.
Trademarks | Privacy Policy | Terms of Use