REG104 - If the input of the REG104 is shorted to GND, will the output feed current back to the input?

Question/Problem:

If the input of the REG104 is shorted to GND, will the output feed current back to the input?

Answer:

Yes, current will feedback through the body diode of the pass FET.

Thanks,

Leslie C.