Hi i currently have an power supply in which i nedd to reduce the noise, and was wondering if the TPS7A4 and TPS7A33 would do the job.
Output power supply +15V and -15V, 65 mA, noise=50mVp-p
I need t reduce it to 100uV and 12V, -12V.
thanks
if not, can anybody recomend an power supply that uses an external battery (12,24,36 and 48)V and outputs from [12,15]V both positive and negative and noise bellow 100uVsqrt(Hz)