Hi, can LM350AT/NOPB (TO-220 package) be used as 1.2V LDO with 3A max current if the Adj. pin is shorted directly to GND? In the datasheet only an application circuit is shown for electronic shutdown application where the output becomes 1.2V when Adj pin is connected to GND using a switching transistor and load draws minimum current at 1.2V. But in my application I want max. current at 1.2V and I am not sure from datasheet whether it can supply it.