Hi,
We are using TPS79101 in our board to generate 3.1 Volts. The input to the TPS79101 is from the Battery charger circuit (BQ24075TRGT). The output of the TPS79101 is used to power an MSP430 and an capsense controller.
When we apply a +/-4KV ESD pulse to the input of the battery charger circuit which has a ESD diode (PESD5V0X1UAB) placed we could see the output of the TPS79101 will become 1.5 Volts instead of 3.1 Volts.
The schematics of TPS79101 is as below.
Request your inputs on this.
Ravindranath R