I need LDO with Ultra-Low Quiescent Current < 10uA
output voltage = 3V
output max current < 100mA
input voltage 0-8V(or more)
any advices?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I need LDO with Ultra-Low Quiescent Current < 10uA
output voltage = 3V
output max current < 100mA
input voltage 0-8V(or more)
any advices?
Lukasz,
We have several different devices that would meet most of those specifications, except for a Vin, min at 0V. Our parametric search is an easy way to try and narrow down to just a few of those choices, and I've input the parameters that you specified in the below search. You can use the add/hide parameters button to narrow down the search more, or search for a different set of parameters.
http://www.ti.com/lsds/ti/power-management/linear-regulators-ldo-products.page#o4=ACTIVE&p32=1&p236typ=0.0005;0.01&p1154=3;3&p451max=0.005;1&p238max=7;30&columnOrderString=o1,o4,p32,p182,p238min,p238max,p1154,p634min,p634max,p451max,p1130,p236typ
Regards,
David Hopkins