Hello
My customer are using TPS51206 for DDR3 at Base Station.
I have a question from Customer. I'd really appreciated it if you could support me.
From Datasheet, VTTREFTOL is as below.
|IVTTREF|< 10 mA, 1.2 V ≤ VVDDQSNS < 1.5 V min48.75% max51.25%
This mean that VTTREF is min666.5mV and max683.4mV at VDDQ=1.35V.
My understand is correct ?
If my understand is correct, could you please let me know the actual performance of VTTREF.
I don't need you guarantee.
My customer need actual perfomance of VTTREF when they calculate at worst case/condition.
Thanks
Best Regards
Koji Hori
Marubun