Hi All,
I have a basic question with regard to functioning of TLV71730P LDO.
This is a 3V fixed output LDO functioning from 1.7V to 5.5V max.
By above is correct to say that:
The LDO shall output 3V when the input is greater or equal to 3V and
when input voltage is less than 3V, is it correct to say that Output Voltage shall be equal to input voltage?
E.g.
Output Voltage = 3V for Input voltage = 4V
Output Voltage = 2.5V for input voltage = 2.5V
Thanks and Best Regards,
Shantanu,