I am looking for clarification on the current sense and programmable current limit options for the TPS7H1101-SP linear regulator. Between the datasheet and application note, I have come across numerous values for the scaling factor of Ics/Iout. 47394 is in the table, 49917 is in the text and plot of the eval board documentation, then another plot on the datasheet shows three curve providing 48065, 47935, 48150. I understand there is some variability from part to part and operating conditions. The datasheet on pp. 19 discusses PCL and uses a CSR value of 47394 for this calculation. But defines CSR as Ics/Iout. Wouldn't we want Ipcl/Iout, why is CSR defined in this calculation with Ics? Is Ics/Iout and Ipcl/Iout the same? For the high side current sense section on pp. 20. The equation uses the same CSR and a Voffset. But Voffset is in amps, just want to clarify this is really an Ioffset. Also, it appears the Ics offset is 5uA, which would correspond to 0.237 A (5uA * 47394), not 0.1899 A in the datasheet. Could you help clarify the value of Ics/Iout and Ipcl/Iout and the appropriate offsets?