Can you please clarify if the TPS715xx can handle a negative ESD event? The datasheet doesn’t
say +/- for the ESD rating, it only shows a positive value for ESD and shows an Abs Max range down to just -0.3V. The customer has added a TVS to help with the negative ESD event, but it doesn't clamp as low as -0.3V, it's closer to -10V. Can it handle -10V at 100-200mA for a few microseconds?
Thanks, Jason