According to the datasheet, the LM1117 is available in 2 different temperature grades:
LM1117-N: 0°C to 125°C
LM1117I: −40°C to 125°C
The output voltage specifications (Min/Typ/Max) for the 3.3V fixed voltage devices are
3.235 3.300 3.365 V (for LM1117-N),
3.168 3.300 3.432 V (for LM1117I).
These values apply over the respective full temperature range.
My question is:
At first glance, the LM1117I seems to have wider output voltage limits. But I wonder if it will have the same limits as the LM1117-N, as long as it is operated in the LM1117-N's temperature range (i.e. above 0°C).