We received the following from a TI FAE regarding the AN1112:
“LP2985 YPB is a 5 bumps, 0.5mm pitch WCSP with small solder balls.
Recommended NSMD land pattern is 0.165 +/- 0.02 mm
Solder Mask Opening is 0.265 +/- 0.02mm
We don’t want the solder mask opening to be too large to avoid
losing solder to the traces connected to the soldering pads.
The SMO in the current App Notes (0.35 +/- 0.025mm) is too large
that need to be updated. “
Can we get confirmation this is correct?