Hi Team,
Our customer are studying LP5907 at the following conditions.
So, LP5907 is used at the back of DC-DC converter.
Therefore, they would like to know the PSRR of the range from 1MHz to 2MHz.
Could you please send it to us if you have this graph?
<LP5907 conditions>
-Vin=3.25V
-Vout=2.9V (or 2.85V)
-Iout= up to 250mA
Regards,
Kanemaru