I want to parallel a number of LP5900 outputs, not for increased current, but for better redundancy and avoiding a diode voltage drop. Each one is fed from a separate LiIon cell. Any single one can supply enough current, but if one cell fails, the 3.3V regulated should still be there.
Questions:
Normally parallelling regulator outputs is a no-no, unless something is done to encourage current sharing. I am more concerned about stability- would the circuit oscillate?
If any cell fails short, would there be any back current through the LP5900? There would be no diode (trying to avoid the extra drop).
I have a drawing, but don't see an easy way to add it..