This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS7H1201-HT

The rated output current is 0.5A for -55C to 210C temperature range. I have 3.3V input, 2.5V output, 0.6A at 70°C. Is the part capable of doing this?