Hi,
I am having a d.c. power source, which while connecting with amplifier circuit introduces noise. I want to design a circuit which will provide a highly stable power supply voltage (6 V). Kindly suggest me.
-- Nishant
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I am having a d.c. power source, which while connecting with amplifier circuit introduces noise. I want to design a circuit which will provide a highly stable power supply voltage (6 V). Kindly suggest me.
-- Nishant
Hi Nishant,
In order to help narrow down the options, could you provide more information about your system. I see that you want 6V as the output of the LDO. What is the input? How much current will the load require?
Below please find a link to a useful tool to help narrow down the LDOs based on your application requirements.
http://www.ti.com/lsds/ti/power-management/single-channel-ldo-products.page?
Very Respectfully,
Ryan
Hi Ryan,
The input to this circuit is also 6 V d.c. directly feeding from a d.c. source. The load current will be approximately 0.15 A. Basically, I do not want to change amplitude of the signal, but to remove noise from d.c. power source and get a stable power supply up to 6.000 V.
--Nishant
Hi Nishant,
In order to realize the benefits of an LDO there needs to be some headroom (Vin - Vout). Without this headroom, the LDO would be in dropout and any PSRR benefit would be severely degraded. Take a look at TPS79901. This device can fulfill your requirements with only 90mV (typical) of dropout.
Very Respectfully,
Ryan