Hello,
I've made a powersupply with the LM1084-adj I switch between different resistors, between GND and Adjust pin. A couple of times I destroyed the LM1084 with switching, it gives after that the full input voltage at the output. I suggest that it is not ok to leave the adjust pin's open, while switching between different resistors?
Between output and adjust I use 240 Ohm resistor.
I build a new one and connect a 100KOhm resistor between the adjust pin and ground, parallel a switch with the different resistors. Is the value from 100KOhm a safe value, or do I need lower resistance? I'll hope anybody can advise me.
Thanks, Hans