My customer evaluate TPS51206 for DDR3L termination.
There is mentioning of Vref tolerance in data seat P7.
- How much is the Vvttreftot in case of |IVTTREF|<1mA and Vvddq=1.35V?
(Is it smaller than 49%-50%?)
Best regards,
Noda
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
My customer evaluate TPS51206 for DDR3L termination.
There is mentioning of Vref tolerance in data seat P7.
- How much is the Vvttreftot in case of |IVTTREF|<1mA and Vvddq=1.35V?
(Is it smaller than 49%-50%?)
Best regards,
Noda
Hi Noda,
Yes, it will comfortably be within 49%-51%.
From the electrical specification at 10 mA it drops worst case 15 mV or to about 48.89%. From Figure 7 about 5 mV of the change in voltage comes from the regulation across load from 1 mA to 10 mA. This means at 1 mA the worse case should be about a 10 mV drop. A 10 mV drop in VTTREF puts it at about 49.26% worse case.
Best Regards,
Anthony
Hi Anthony
Thank you for the reply.
I have a little more question.
Is the same thinking also the shift in + side?
How much is VTTREF shift in -1mA to -10mA in fig7 ?
Best regards,
Noda