Hi,
I'd like ask about the Figure 27 & 28 in TPS75801 D/S.
What does the "Copper Heatsink Area" mean?
Does it mean the 1 oz. Copper Ground Plane in Figure27?
Thanks
Go
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Go,
Nice catch on the units - it is 1cm by 1cm. Under the conditions above the maximum ambient temperature is 55C as there is a large rise in junction temperature. I would advise trying to stay quite a bit under this limit as high temperatures (125C) are known to decrease the lifespan of the IC.
Regards,
David
Hi, David
Thank you for your comment.
please let me know about Figure27 in TPS75801 D/S in a little more details.
1. Is the area indicated in red also copper plane? if yes, what is the area of it?
(Please see the attached file)
2.Are the area indicated in green also thermal vias?
It doesn't seem to connect to Copper Solder Pad on top side, is it right?
(Please see the attached file)
Thanks
Go