later, I used TPS54332+TLV1117-33 as the power module of analog part on the DSP board . The schematic is shown fig. 1 in attached pdf file. The input voltage of TPS54332 is 12VDC, output voltage is 5VDC connected to input of TLV1117-33. The noise and ripple of TPS54332+TLV1117-33 are shown fig. 2 and fig. 3 in attached pdf file, respectively. At last, I show the noise in ADC input pin as fig. 4 in attached pdf file. The measured noise in ADC input is agree with the sampled noise of the ADC.
Now, my question is how to how to reduce the sampled noise of the ADC. In addition, What is the relationship between sampled noise and regulator output noise?
best regards.