Hi Team,
They would like to apply the external 5.1V to the out pin when this device is disabled.
I understand that they can apply the external 5.1V to the out pin because this voltage doesn’t exceed the absolute maximum.
However, they worry about current of discharge resister(230ohm).
This current is around 18mA (5.1V/230ohm) if this device is disabled and the voltage of out pin is 5.1V.
I understand that this current doesn’t adversely affect this device.
Could you please let us know if you have any concern?
Regards,
Kanemaru