This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC283 PIN CT

Other Parts Discussed in Thread: UCC283, TPS54386

Hi,all

    Now I use UCC283 to regulate DC8.5V-DC8V @2A. I find that CT pin is not pulled up by device.

    "If the CT pin is not pulled low, the IC internally pulls up the pin enabling the regulator. The CT pin should not be forced high, as this interferes with the short-circuit-protection feature. Selection of the timing capacitor is explained in Short-Circuit-Protection." I just connect this pin to GND with a 680pF CAP. The output is 0V and the ADJ pin is 0V, I think UCC283 is not working. How can I connect this pin?  UCC283 don't need the shut down function.

Thanks 

Jacky