REG103GA-3.3/2K5 on an old design is now failing during abrupt application of +12V. The 3.3V output is minimally loaded at about 7-10mA. This hard failure causes VOUT to match VIN which destroys a microcontroller.
With the microcontroller removed, I've reproduced the failure using a 470 ohm resistor.
Using a bench supply set to 12.0V. REG103GA-3.3 circuit has V enable tied to VIN and C-NR is connected 0.1uF to GND. Tab is not electrically connected. VOUT load is 470 ohm resistor and about 10.2uF of capacitance. The 10uF is ceramic but is about 2 inches of PWB trace away so the ESR should be approaching 100mohms.
I have also seen the original failure with the 10uF removed and with the NR cap changed to 0.01uF.