Hi
we had been using the TPS7A8001 for our designs but that one only goes to 1A, I have been trying to find something similar with similar or better noise and pssr specs but with 1.5A or higher current, but no luck so far.
any suggestions ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
we had been using the TPS7A8001 for our designs but that one only goes to 1A, I have been trying to find something similar with similar or better noise and pssr specs but with 1.5A or higher current, but no luck so far.
any suggestions ?
HI
Thx for he answer. Is that the only choice for >1.5A current? Is there a way to use the internal resistor divider resistors of TPSA8300 with an external resistor/s to improve the adjustable output voltage resolution to say 10mV or finer, the default settings just gives 50mV of adjustability.
Also, is there any recommendation on choosing the resistor value ranges to reduce parasitics/noise. Usually one of the resistors has a fixed recommendation and the other will be adjusted to get the desired range.
Also is there another part without the 5 programmable voltage pins in a smaller package with very good PSRR and noise specs ?