I have a board using the LP2951-33D LDO regulator for a 3.3V power supply.
When powering the board, and measuring the output voltage, it is approximately 2.5V, with a 5V input voltage.
I have tested 2 boards. Actual measurements for 1 board: 4.98V in, 2.48V out
The LDO has SENSE and OUTPUT connected together, as well as VTAP and FEEDBACK are connected together.
The main load on the 3.3V supply is a TIVA-C TM4C123GH6PZI MCU.
My load estimated for the 3.3V is 85 mA.
I suspect that the LDO may be overloaded; however, the consistent 2.5V on 2 boards is strange, and the chip does not feel hot when I touch it.
Any suggestions for anything else I can look into?