Dear sir,
We are testing TPS7A1601 for 15V output with following parameters:
Vin= 20V
Cin = Cout = 2.2uF
Feedback resistors: R1= 12M , R2=1M
At EN (Enable) Pin, I am applying 5V from a battery.
PG, NC, DELAY pins are left floating.
GND is connected to ground of Power supply.
But we are getting only 1.5-2.5V at output.
The EN pin is floating initially, then 5V is applied for some time and then 5V is removed.
However, there is no change in Output due to Enable pin.
The FB pin has 1.2V.
Scope file is attached for your reference.
Channel 1 is Input
Channel 2 is Output
Channel 3 is Enable (It floats from 12- 17V)
Kindly suggest the changes required at your earliest.
Regards,
Gaurav Tarkas