Hi Team,
Our customer would like to use LP2951CSD/NOPB (WSON PKG) at the following conditions.
[Customer conditions]
-Vin=24V
-Vout=12V
-Iout=60mA
-Pd=(24V-12V)*60mA=0.72W
-θJa=43.3℃/W
-Ta=70℃(max)
We believe that they can use LP2951CSD/NOPB at this condition.
Because, “Tj=Ta+(θJa * Pd)=101.2℃” at this condition.
However, according to “Figure 27. LP2951-N Maximum Rated Output Current” of the datasheet,
We can’t use this device…
Therefore, I would like to know whether this device is usable.
Regards,
Kanemaru