Greetings,
I would like to suppress noise and especially ripples for the 15 Volts power supply of a sensitive detector. We currently experience detrimental ripples at ~320 kHz that are picked up by our downstream data acquisition, despite using a low-noise power source. I thought of using LP38798 voltage regulator, which can handle 15 Volts as well as the expected 50 mA currents and exhibits an impressive PSRR well into the MHz range. However, we only need a few regulated power supply units, and would like to build a prototype on an ordinary solderless breadboard.
Can you please advise whether LP38798 can be mounted on a solderless breadboard using any of the following Schmartboard DIP adapters?
http://schmartboard.com/schmartboard-ez-0-5mm-pitch-10-pin-dfn-to-dip-adapter-204-0022-01/
http://schmartboard.com/schmartboard-ez-qfn-10-and-32-pins-5mm-pitch-2-x-2-grid-202-0017-01/
Evidently these two options offer only 10 pins, but I hope legs 1 and 12 can remain unconnected given the low currents involved.
Alternatively, can you please suggest other mounting solutions, or other voltage regulators that can handle 15 Volts and are easier to mount on a breadboard?
The same question applies for a LP3878-ADJ voltage regulator which I thought of using in the same circuit, for an adjustable 0-900 mV supply with uA currents. If that won't work I'd opt for the LP5907 regulator, reducing its output voltage with a voltage divider.
Thanks in advance,
Lior