I have a TPS 73801 with a 10 MicroFarad on the input. The enable is connected to the input voltage. R2 is a 1.3kilo Ohm, R1 is 590 ohms. I have 9.12volts coming in and the resistors should limit the outgoing voltage to 7.77volts. The measured voltage is 3.87 voltage on the output side. I had to solder 4" leads to the terminals for use on my breadboard. Do you think I may have fried the voltage regulator. Any clue as to why my voltage is so low. Thank you.