Dear Technical Support Team,
I have a question about LT1009IDR.
Dose aVZ spec of datasheet include ΔVZ(temp)?
I think that 2.525V and 2.475V(Full range of D/PW package) includes ΔVZ(temp).
(Change in reference 15mV from Vz of 25℃(min 2.49 / max 2.51 max))
So I tried to calculate from -40℃ to 85℃ for LT1009IDR(D package).
|aVZ| =(((2525-2475mV)/2500mV) x10^6) / 125℃= 160ppm/℃
But it didn't much aVZ spec of datasheet (typ 20,max 35 ppm/℃)
How should I calculate correctly?
Best Regards,
y.i