Hi,
I am powering my LASER diode using a constant current source (LM134) in which the output current is set using a set resistor. I want to soft start (gradually increase current from threshold to optimum)the LASER diode by gradually decreasing set resistance value.
Can I do this using a digital potentiometer as set resistance of the current source?
If yes, the set resistance value should be in the range of 150 ohms to 30 ohms with a step size of 1 ohms, which is the suitable digital potentiometer for such an application?
Regards,
Nidhi Singh