This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP3856ESX-ADJ vout maximum rating <urgent>

Other Parts Discussed in Thread: LP3856

Dear Sir,

I am using LP3856  (low drop voltage LDO)for our design of vin 6.7V vout 6.2V / 2A. 

we check the datasheet and the page 3 mention Output Voltage (Survival), (4) , (5)  -0.3V~ +6V 

(4) If used in a dual-supply system where the regulator load is returned to a negative supply, the output must be diode-clamped to ground.

(5) The output PMOS structure contains a diode between the VIN and VOUT terminals. This diode is normally reverse biased. This diode will get forward biased if the voltage at the output terminal is forced to be higher than the voltage at the input terminal. This diode can typically withstand 200mA of DC current and 1Amp of peak current.

Can this part work for vout 6.2V? We need to confirm this specification of output voltage maximum. please kindly let me know . it is very urgent , Thanks.