Hi there,
We are using the TLV70233DBVR with +5V in the input. We have two 1uF/6V3 X7R, one on the input and other on the output. The load capacitance at the output is composed by a 10uF/100nF/10nF/1nF in parallel.
What we are experiencing is that at startup the regulator works ok, regulating the output for 3V3, after a few seconds(1~2) it ramps up to +5v, after some seconds it starts to regulate again, and it keeps doing this over and over.
We have some other product that is using this regulator with exactly the same load and no issues are seen.
We suspected gnd coupling issues so we improved the ground plane of the chip, even so the problem persists.
Can anyone help in any way?
I tried 100nF in the input and 1uF/X7r in the output, both 1uF, the issue presists....
Thanks!