Hello,
I am after a high side constant current regulator with an enable pin like the lm317, should work up to 80V and over -40 to +125 C.
Automotive safety application, so must be low cost and the solution to use a few as possible components.
The application is to test for defective electrolytic capacitors by charging them up with a constant current and then calculating capacitance 'C' by the voltage rise rate. Capacitor fail by low C, or high leakage current is detectable.
The constant current source should switch ON in a few microseconds. The attached schematic shows a solution using transistors, it is not very good with temperature and there is about a 7mA wasted current in forming the HSS. Capacitor A is charged up to 40V using a flyback transformer in <50mS
What part is suggested?both_14_for_document_report.pdf