I was considering using the TL783 High Voltage Adjustable regulator in a current source configuration for an application where the temperature range is from -40C to 85C. Figure 17 in the datasheet describes the circuit configuration with R connected between OUT and ADJ. The load current will be set to a range between 11mA to 14mA. The input voltage range is between 110VAC and 220VAC. The load will be switched, however quiescent current will be present to power the regulator. The load is roughly 7.2K ~ it controls an external output. The intention is to keep this point at roughly 110V. So the drop across the current regulator will not exceed 125V. Will this configuration operate at -40C? I have read that operation cannot be guaranteed at this temperature but that may be based on operating conditions. Is there a load in terms of current / voltage where the use below 0C will cause the device to not turn on?