Hello Reference Experts,
REF5025 has mentioned in the data sheet information about Parameter Measurement Information and Solder Heat Shift.
Does something similar apply to the LM4132A.. There seems to be mentioned nothing in the data sheet?
Reason for question is LM4132A after mounted on PCB show Vref with tolerances larger than expected max tolerance of +/-0.05%.. measured deviation from 3v3 is -0.302%
Parts are mounted close to edge of the PCB so we don't expect mechanical stress to be the issue leading to the unexpected tolerance of -0.302%