Hi e2e Lin Reg Forum,
I've read about and witnessed a typical failure mode of the TO-220 package voltage regulator in which it keeps signaling, but with an output that is elevated above its normal regulated specification. This obviously can damage connected devices, if the high output of the failed regulator is above their abs. max. tolerance...
Is this a typical failure mode for all linear regulators - even those with the TO-3 package? I'm considering retrofitting an old power supply with crowbar protection circuits and wanted to make sure that this was not going to be unnecessary, since I don't want to disturb the original circuits otherwise.
Thank you...