I am confused by the data sheet for TPS7A84 regarding the recommended input voltage range for the EN pin.
In section 6.3 it says that the recommended range for VEN is 0 to VIN.
But in section 6.5 on page 6 it says that VIH(EN) is 1.1 to 6.5 V. Is the 6.5 V only applicable when VIN = 6.5 V? Should it not say 1.1 to VIN instead of 1.1 to 6.5 V if that were the case?
The absolute maxim ratings says that VEN(abs max) is 7.0 V. Is this under the condition that VIN is 6.5 V or maybe 7.0 V and that a lower abs max rating applies for lower VIN?
It would be convenient for me to be able to drive VEN with a 3.3 V signal in an application where VIN is 1.5 V (and VBIAS is 5V). Is it OK to apply 3.3 V to VEN under these conditions, or must I limit VEN to 1.5 V?
(On a side note, there are two typos in the data sheet on page 6. On the row for VIL(EN) it says "EN pin high-level input voltage" when it should say "EN pin low-level input voltage". The same but opposite error exists on the next line.)
Per