Hi Sir,
I would like to know about LP5907-3.3 dropout voltage define. In datasheet P5, it max. 250mV @ Iout = 250mA.
So, If I set I want to keep Vout can always not lower than 3.3V, I just need keep Vin = 3.3 +0.25V = 3.55V, right?
because I saw the section 6.5 as below, or it mean other spec based on this test condition?
Thanks!
Jeff