Hi,
One of my customers is looking to use a combination of LDOs to share a load of 10A (8A typical). They want to use LDO in order to attain a high PSRR of >30dB till 10MHz. The input voltage would be around 0.5V to 1.2V higher than Vout which is adjustable too. The typical outputs needed would be 0.9V, 1V, 1.2V, 1.8V and 2.5V. I looked for LDOs with current sharing feature and found only TPS7H1101-SP which is not needed here.
Can you please suggest any LDO or an implemented solution for this application?