My customer needs help with TLV70718PDQNR
1) Continuous Power Dissipation (W)
2) Rated operating ambient temp (˚C)
Do we have such data ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Naser,
LDOs are power dissipative devices rated over a operating junction temperature range. Continuous power dissipation (PD) and ambient temperature (Ta) can be calculated using the junction-to-ambient thermal resistance (Θja):
Tj(max) = PD(max) * Θja + Ta (max)
From the Recommended Operating Conditions table and Thermal Information table we can find Tj(max) and Θja:
125 = PD(max) * 208.1 + Ta (max)
At this point, we have one equation and two variables. Typically a customer knows either the max power dissipation for their application ((Vin - Vout) * Iout) or the max ambient temperature for their application.
Very Respectfully,
Ryan