Hi
We have a chip done as part of research project. Need to provide 3.3V supply for IO and 1.2V for core. Input voltage is 5V tapped from USB. Chip current requirement is less than 500 mA. If the power supply IC can also provide clock more than 10 Mhz (max 100 Mhz), that is also desirable.
So high level spec is
Vin Nom = 5v
Vout1 Nom = 3.3V
IOUT1 = 500 mA
Vout2 Nom = 1.2V
IOUT2 = 500 mA
Nice to have : Clock output with 10 - 100 Mhz range.
Please help me to chose right device.