Dear all,
Could you teach us what peripheral elements is needed when we do not use power-good and use standard watch dog?
My idea of peripheral elements are following. Is this correct?
pin 1[IN]: Input capacitor
pin 4[EN]: no (connect to Vin)
pin 5[FSEL]: no (connect to Vin/GND)
pin 6[WTS]: no (connect to Vin)
pin 11[ROSC]: resistor to set Twd
pin 12[DELAY]: no (open)
pin 13[WD]: no (connect to GPIO)
pin 15[WDO]: pull-up resistor
pin 16[WD_ENB]: no (connect to GND)
pin 18[WRS]: no (open)
pin 24[PG]: no (open)
pin 25[PGADJ]: no (connect to GND)
pin 28[OUT]: Output capacitor
Best regards,